Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you assign output contactor command to R2 relay on an ATV630 drive?
Issue:
Wants to set R2 for output contactor command

Product Line:
ATV630

Environment:
All

Cause:
Can not assign R2 to output contactor command

Resolution:
To assign R2 to output contactor cmd, first make sure R2 assignment is Not assigned. Then go to Complete Settings / Generic Functions / Output contactor CMD. Then set Output contactor assign to R2.    Then go to Complete settings / Error Warning Handling / Output phase loss, and set Output phase loss assign to "No Error Triggered"