Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to modify the external project path for Vijeo Designer ?
The goal of this article is to explain how to modify the external project path for Vijeo Designer if it had been modified or is incorrect.
The article is applicable for Vijeo Designer v6.2 or more.

For example, it's possible to install Vijeo Designer software on a system disk (as C:\ ) and store the project on another disk (as D:\ )

To modify paths, please use the regedit tool and modify 2 registry keys in the registry base :
  • " Vijeo-frame -> Vijeo-Manager -> ROOTDIR "
  • " Vijeo-frame -> Configuration -> VijeoManagerDir "
VJD_Registry_path_01VJD_Registry_path_02

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: