Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
My Site Energy Consumption is not equal to the sum of usages or zones
If the submeters are not metering 100% of the load, the total energy will be lower than the sum of submeters.
If there are sub-sub meters, make sure you do not double count the load:
Example:
  • Main Meter
    • Meter 1
      • Submeter 1.1
      • Submeter 1.2
    • Meter 2
      • Submeter 2.1
      • Submeter 2.2
If you define usage for Meter 1, Submeter 1.1 and Submeter 1.2, you will double count Meter 1 value.
In that case, you should not define usage for Meter 1.

Usages