Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between media converter P2M & P2ML products used with Easergy Micom P54x differential relay?

Issue:
Different between media converter P2M & P2ML products using along with Easergy Micom P54x differential relay

Product Line:
Easergy Micom P54x device

Resolution:
P2M device was Areva supplied product (old one ) and P2ML is Schneider make product.

P2ML has LCD display However both the model has 2 variants like (A & B) which has its own requirement of selecting fiber and protocol baud rates.
Please refer the manual with the existing device at site and make the proper selection of cables and baud rate settings accordingly.

Please note that P2M Areva make is no longer available.

Schneider Electric Saudi Arabia

Attachment(s)
p-2m-usermanual-v22_compress.pdf [282.67 KB]
P2ML_EN_M_B11_.pdf [1.24 MB]