Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
APM Technical Support for Canada - APM Partners authorized in Canada

Issue: Customer needs technical support for APM drives in Canada

Product line: APM, ATV6A0 APM, ATV9A0 APM, ATV680 APM, ATV980 APM, ATV 6L0 APM, ATV9L0 APM

Resolution:

Altivar Process Modular (APM) drives are a version of the Altivar 600 and Altivar 900 series drives assembled and packaged by approved third party partners.  The partner is responsible for designing, building and selling the APM Drive.
The APM drives are offered in 380-480 volt (150 thru 1100 HP) and 500-690 volt (125 thru 1200 HP).

Schneider Electric Drive Products Support can be engaged for normal programming/troubleshooting assistance if needed at 1-800-565-6699.

Any issues or concerns related to purchase, design, delivery, manufacture or warranty of the APM drives should be directed to the Partner.

Below is the table listing the APM Partners in Canada, authorized to support the APM Drives (as of January 2022).

List of the Canada Partners

However, we have few APM SI/OEM who have access to APM and buy from our distributors and sell to their customers.

Here is the list :

Automation Now

Celco Advancing Automation

Delco Automation

Softac Systems

Watertek

Tusk Automation

PowerOn Control Systems

Please note below list may change in 2025 as we are formulizing the APM SI membership agreement in the country and will add/remove few SI in 2025.

1