Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any added value to having the Ethernet/IP data being processed in the FAST task
The exchanged data between the scanner and the application is made at the rate of the Mast task. But this exchanges may be interrupted by higher priority task than Mast (by the Fast task for example). So, all input DIO data computed in Fast task are not guaranteed to come from the same inputs scan cycle and all output DIOs data are not guaranteed to be sent through the same next Mast cycle.

There is no added value to compute data in a Fast task if the data to be sent/read behaves similar to a DIO scanning system.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre