Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot find the IEC_BMDI block in the Types Library Browser

The issue has been fixed in the UMAC v3.0 Update.

  • Download and install the UMAC v3.0 Update from:

https://www.se.com/us/en/download/document/UMACv3.0/

  • Open the 'Unity M580 Application Converter'.
hgj
  • Click on About.
yujj
  • Click on Install library.
  • Close the  'Unity M580 Application Converter'.

ytr

  • Start Control Expert.
  • Create an M580 project.
  • Open the Types Library Manager.
  • Search for IE*
  • The block will be shown:
ett