Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the IP addresses set by default in Harmony STM6 Edge Box HMISTM6BOXIOT?
The HMISTM6BOXIOT is a gateway which can be used only without screen touch. The configuration menu is accessible only using specific IP addresses.

The goal of this FAQ is to provide you the default IP addresses confgured by default in our product.

The FAQ is applicable for HMISTM6BOXIOT.
table

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: