Answer:

For further information, please refer to operator's manual 381333-163 or contact 1-800-800-2726 then dial 3 for Technical Support.
1. The Automatic Generator Exerciser automatically exercises the generator for 20 minutes once every 14 days.
2. Press and release the Automatic Generator Exerciser button. After about 8 seconds the exerciser light flashes 14 times to indicate that the exerciser has been set. The number of flashes indicates the number of days until the next exercise period (at approximately the same time the button was pressed).
For further information, please refer to operator's manual 381333-163 or contact 1-800-800-2726 then dial 3 for Technical Support.
Released for: Schneider Electric Saudi Arabia