Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to order cover kits for the controller and meter on UL Type 3R enclosures.

In applications where there is prolonged exposure to direct sunlight (UV), the use of double-door Secure UL Type 3R enclosures (code ‘M’ in the catalog string) is recommended so that the controller and meter front faces are protected by the outer door.  If a standard, non-secure UL Type 3R (enclosure code ‘F’) was ordered, cover kits can be purchased and field-installed to provide protection in the absence of the outer door.

The orderable kit numbers are the following:

K1200209-001
ATS METAL DOOR COVER KIT FOR
GROUP 5 OR GROUP G IN NON-
SECURE 3R ENCLOSURE

Includes:
  • hasp
  • protective door cover
  • Installation instructions
Controller Cover Kit



K1200209
ATS METAL DOOR COVER KIT FOR
5210 OR 5220 METER IN NON-
SECURE 3R ENCLOSURE

Includes:
  • hasp
  • protective door cover
  • Installation instructions
Power Meter Cover Kit

To order the cover kits, please reach out to ASCO Parts at parts@ascopower.com or dial 1.800.800.ASCO (2726) and follow the voice prompt to select the Parts Department.

To request a digital copy of the related Installation Manual 381339-330, please reach out to technicalsupport@ascopower.com or dial 1.800.800.ASCO (2726) and follow the voice prompt to select Technical Support.