Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why doesn't eSetup detect the EVlink Pro AC ?
Check that the EVlink Pro AC is powered ON with the strip light green.
Check that you are close to the EVlink Pro AC, less than 15 meters away.
Check that Bluetooth is activated on your smartphone or tablet.
Check that you have not entered 3 faulty pin codes.
Check that you have the right name of the charging station.
If the above is OK, it means the Bluetooth is not active on the EVlink Pro AC, in which case you can:
1- Activate the Bluetooth by powering the charging station Off and then On, and wait for the strip light to turn green.
2- Tap the admin badge on the RFID reader. The Bluetooth of the EVlink Pro AC will be activated for 2 hours.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre