Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the communication settings on EVlink Pro AC to connect an external Power Meter on an RS-485 bus ?

Article available in these languages: Czech

The settings are: 9600 baud / Parity Even/stop bit:1 / Do not use the slave address 247.