Yes, depending on the product commercial reference, see in the catalog description, EVlink Home is compatible with TIC (Linky: only historical mode). The anti tripping module ref EVA1HPC1 (1P+N) or EVA1HPC3 (3P+N) can be used with the references that are not compatible with TIC to prevent the main incomer circuit breakers from tripping.
Released for: Schneider Electric Saudi Arabia