Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many Ethernet ports are on the ATV340 E suffix Drive?

Issue:

Ethernet ports are on the ATV340 E suffix version Drive?

Product Line:

ATV340 with E suffix only.

Environment:

All

Cause:

Are both ports active for TCP or IP?

Resolution:

Yes The ATV340E drive has two Ethernet ports for both TCP or IP programming.

ATV340 Ethernet data sheet