Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Requesting the Altivar drive motor overload trip curve.

Issue:

Requesting the trip curve for the motor overload protection feature of the Altivar drives.

Product Line:

ATV12 ATV212 ATV320 ATV340 ATV600 ATV900

Environment:

All models

Cause:

Estimating trip time

Resolution:

All of the Altivar drives provide motor overload protection based on standard IEC947-4 and therefore use the same trip curves. Please see the attached file.

Schneider Electric Saudi Arabia

Attachment(s)
Altivar thermal protection curve.pdf [658.13 KB]