Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to configure the Harmony Edge Box HMISTM6BOXIOT to send data in SQL Database?
The goal of this FAQ is to share some complementary documentation and demo project to connect HMISTM6BOXIOT to SQL Database.

This article, demo and manual are applicable for HMISTM6BOXIOT with EcoStruxure Machine SCADA Expert 2020 SP2 (minimum).

The Demo project: https://schneiderelectric.sharepoint.com/:u:/s/BoxSupportL3Group/EQPSIH_zxHlCudO-C2R8jlkBnR1-RkDpYOmoeVe_1MLmwg?e=QwPXWa
The Demo Setup Guide: https://schneiderelectric.sharepoint.com/:b:/s/BoxSupportL3Group/EQpjjCwejHNIi7AH-1Cj2HoBryrcCS4Jz22sOOPYJZF1uA?e=WTmZYu

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: