Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Ecostruxure Process Expert[2021]: Unable to connect simulator from remote Engineering Client.

This document explains user what needs to be done when User wants to connect to a Simulator from Remote Engineering Client.

When User Runs a simulator on Engineering Server Machine, by default the simulator will run with 127.0.0.1 IP address with a port defined like 502. If user wants to connect the Simulator from Remote Engineering client, then he will not be able to connect.

pc1

In order to have connections from other PCs to Simulator, User need to change the Simulator IP address from 127.0.0.1 to its own host IP address.

pc2