Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the joint pack for AP2516G10ST?

Issue:

Needs the correct joint pak for AF2516G10ST busway

Product Line:

I-line Busway

Environment:

AF2516G10ST

Cause:

Needs new joint pak

Resolution:

The joint pak for the AF2516G10ST is number AF2516GJP

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre