Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the OPCUA client function block in Control Expert access the OPCUA server module BMENUA0100 via the backplane port?
Issue:
OPCUA client function block in Control Expert accessing the OPCUA server module BMENUA0100 via the backplane port


Product Line:
EcoStruxure Control Expert


Resolution:
No. The OPCUA client function block can access the UA server only by the external port of the BMENUA0100 module or the embedded Ethernet port of the CPU