Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M580 counter modules

Issue

Using the Modicon M580 family I would like to get input from a 5VDC incremental encoder to track position. Is there an input module I can use for this? If not, what other options do I have? If I convert the 5VDC to 24VDC is there a input module that can track a 24VDC quadrature input?

Product Line

Modicon M580, Modicon X80

Resolution

We do not have a 5VDC module for an incremental encoder. If you have a 24VDC signal, we do offer the BMXEHC0200 which supports quadrature.

Here is a link to a YouTube video on the subject. https://www.youtube.com/watch?v=cNf5adjfBFE

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: