Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SCADAPack x70 MB_IP_MASTER Logic Editor Example
When using a SCADAPack x70 device it is recommended to use the Modbus Scanner implemented with RemoteConnect for simple Modbus polling of a server device (Modbus RTU or Modbus/TCP).

It may be desirable to have more control with the use of a logic program to perform the Modbus Client operations. An end user can use the MB_IP_MASTER block in the logic editor to perform these tasks.

This example shows how to implement a typical Modbus read/write sequence in logic with retries and error detection. it uses a combination of LD (Ladder Logic) and FBD (Function Block Diagram) for section execution. This example can be adjusted for Enron Modbus, yet the example showcases standard Modbus

This example includes Client and Server projects for SCADAPack x70 using RemoteConnect

Schneider Electric Saudi Arabia

Attachment(s)
SPx70_ModbusTCP.zip [211.19 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre