Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a PM5500 series meter have a Modbus TCP/IP and BACnet IP master connection simultaneously?

Issue
A customer needs to connect one PM5500 meter to two different sites using two different protocols.

Product Line
PM5560, PM5563

Environment

Communications

commissioning

Resolution

BACnet and Modbus are different communication protocols.

  • BACnet is a broadcasting protocol where devices continuously listen to the master. When their turn (token) comes, they respond to the master.
  • Modbus, on the other hand, is a request/reply protocol that provides services defined by function codes. These function codes are elements of the Modbus request/reply Protocol Data Unit (PDU).

The PM5500 meter can communicate with both systems simultaneously without any issues.

PM5000 series meter documentation: FA234023

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: