Issue
Link local IP address error
Product Line
EcoStruxure Control Expert
Environment
EcoStruxure Control Expert
Resolution
The error you are getting is because you are trying to configure the IP Address on the Link-Local subnet range. Also known as Automatic Private IP Addressing (APIPA). This is reserved IP for 169.254.0.0/16 (169.254.0.0 - 169.254.255.255). This subnet block is reserved for devices to use in the event an IP Address cannot be assigned through proper channels like DHCP.
Released for: Schneider Electric Saudi Arabia