Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the certifications for the PMEPXM0100 X80 Profibus module?
Issue:
Certifications for the  PMEPXM0100 X80 Profibus module


Product Line:
PMEPXM0100


Resolution:
The X80 Profibus module is certified for: CE, CB Safety UL, CSA, ATEX, FCC-ICES, PI

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: