Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Auxiliary Contact Blocks Be Mounted When Using GV2GH7 Line Spacer?
Issue:
Using the GVAE auxiliary contact blocks when GV2GH7 line spacer is used on GV2P Motor Circuit Breakers

Product Line:
GV2P, GV2

Environment:
Contactors and Starters

Resolution:
Front mounted auxiliary contact blocks (GVAE**) when a GV2GH7 line spacer cannot be mounted. Recommended to use the Left Hand Side Mounted auxiliary contact blocks (GVAN**) instead.