Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why doesn't the Vijeo Designer's Security Inactivity Timeout bring me to the specified panel?

Issue: I configured the Inactivity Timeout under the Security node of Vijeo Designer, but the screen does not change to the specified panel after the timeout.

Product Line: Vijeo Designer programming software

Resolution: In order for the Security Inactivity Timeout to work as desired, you must make sure that the Security Level for all panels is set accordingly (except for the panel that should be navigated to after the timeout).

For example: Here below all the panels previously didn’t have a security level assigned to them. It was set to "Security Disabled". If you want the inactivity timeout to bring you back to the panel 3, (for example) you need to set the Security Level for each panel as shown below:

Security Level

The only panel that shouldn’t have a security level is Panel 3 as you want to be able to access that panel with no security rights. The security level for the other panels can be set to Operator or Administrator, depending on the level of user rights.