Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the scale of the Altivar Process Drive Analog output AQ1 when assigned as motor Frequency?
Issue:
Need to know the scale of the ATV600 and ATV900 Drives Analog output AQ1 when assigned as motor frequency.

Product Line:
Altivar Process ATV630 ATV650 ATV930 ATV950

Environment:
All

Cause:
Need to know how the analog output correlates to motor frequency.

Resolution:
The default scale is 0 - tFr (Max Frequency).
Note that the drive's High Speed Setting (HSP) may be same or different.

Example:
ATV630 has HSP = 50Hz and tFr = 60Hz.
AQ1 assigned as 4-20mA output for motor frequency.
motor frequency at 0Hz = 4mA output
motor frequency at 60Hz = 20mA output
It is a linear relationship between these endpoints.

The scaling can be changed with parameters ASL1 and ASH1.  See the Programming Manual for details.