Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the altitude derating of standard TM5 IO modules?
The altitude derating of standard TM5 IO modules is the same for all TM5 modules but it doesn't mentionned on the documentation.

TM5 environmental condutions:

temperature TM5 IO modules

The TM5 altitude derating is a reduction of ambient temperature by 0.5°C per 100m:

0 to 2000m => No limitations
>2000m => -0.5°C / +100m