Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
XPSMCMCP0802 USB connection from PC is not working

Issue
I cannot connect my SoSafe software to the XPSMCMCP0802 modular safety controller via USB cable. How do I troubleshoot?

Product Line
Modicon MCM
SoSafe configuration software

Environment
Windows 10 PC connecting to the physical controller

Resolution
Please launch your Windows Device Manager and double-check if the Driver is installed correctly.
In the Device Manager, when you plug in the XPSMCMCP0802 via USB cable, look under "Ports (COM & LPT), it should look like this:
Device Manager - Appearance of XPSMCMCP0802 in "Ports (COM & LPT)"

If you are seeing an exclamation mark on the left icon or it doesn't show up at all, first try to uninstall and reinstall the software - it should reinstall the driver.

If that does not work, download the driver package independently from here:
https://www.silabs.com/documents/public/software/CP210x_Universal_Windows_Driver.zip
(MD5: a727cbd5e6882e97709cbfc1ba42f4ed)

1) Unzip the file to a location of your choice in your Windows file system.
2) Disconnect the XPSMCM controller from the PC's USB port
3) Then follow the installation instructions inside the text file "CP210x_Universal_Windows_Driver_ReleaseNotes.txt" to install the driver
-> Just right-click the file silabser.inf from the root directory, and click Install
4) Once the installation is completed, connect the XPSMCM controller once again.
5) Retest the connection.

If in the event that (a) the driver works for a while, and then stops after a random time or (b) the driver works intermittently across several computers in the same company network, this could indicate that there is an outside agent like an anti-malware / antivirus software blocking it. With newer algorithmic-based anti-malware/anti-viruses, AI algorithms can be intermittently aggressive and you may need to have your IT put the driver into an allow-list.

Schneider Electric Saudi Arabia

Attachment(s)
CP210x_Universal_Windows_Driver.zip [278.74 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre