Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the IG2000CBM the same as IG2000CBMPM

Issue:

Is the IG2000CBM the same as IG2000CBMPM

Product Line:

Medical Products

Environment:

IG2000CBM

Cause:

N/A

Resolution:

The IG2000CBMPM is a variation of the IG2000CBM that is designed for mounting in Square-D panels with no back box required. See below for the IG2000CBM part numbers.

IG2000

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre