Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PLC Simulator for Control Expert

Issue:

Getting an error when launching the simulator:

Can't start communication server.

Default TCP/IP address xx.xx.xx.xx you have set in the option is not a valid IP port for this PC.

Resolution:

Call up Simulator Panel options by right clicking on the avatar and correct the 'Listening IP Address'. It should either be 127.0.0.1 or the ip address of the PC/VM that is running the simulator.
256804_IMG