If SCADAPack Workbench will not Launch, a potential solution is 
- Open Event Viewer
- Go to Event Viewer>Windows Logs>Application
- Determine the Error, see example below
- To Correct the issue, Open the Scadapack Workbench CD installation
- Go to the "\Prerequisites\VS2013 IsoShell" folder from the installation media
- Install the following application manually vs_isoshell and VS12-KB3107629
- After installing the applications manually restart your machine.
Released for: Schneider Electric Saudi Arabia