Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we using ZB4BZ021 on XD4PA14 to achieve flush mounting?

Even if it is possible to assemble XD4PA14 joystick in the ZB4BZ021 flush kit.
It will not perfectly fit : The joystick will be 1 mm above the flush accessory. So it depends on customer's sense of aesthetic !

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre