Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Ports used by PCT server Client application


PCT1 doesn't use TCP port 2512.


Here are listed ports used by PCT1, the customer can block all others ports to be on the safe side.
• TCP on port 4444 (fixed)
• HTTP on port 80 (default)
• HTTPS on port 443 (default)
• Default server port is port 9091
• Engineering port 32768-61000


Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: