Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PowerChute will not connect to Nutanix AHV cluster using SSH key authentication
Issue:
PowerChute Network Shutdown will not connect to Nutanix AHV cluster using SSH key authentication. A connection is made when connecting to the AHV cluster using SSH with username and password. But, when connecting using public/private key authentication, the connection fails.

Product:
PowerChute Network Shutdown

Environment:
PowerChute Network Shutdown on Windows configured with Nutanix AHV.

Cause:
SSH authentication failure when key is created using ssh-keygen on Windows.

Solution:
  1. Use puttygen  (part of Putty toolset https://www.puttygen.com/) to create the keys.
  2. Copy the key to .ssh/authorized_keys on each AHV hosts.
  3. Copy the key to key Prism->Settings->Cluster Lockdown.