Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
License Manager Integrity check failed

Issue:

When launching or installing License Manager an integrity check is reported and it does not open. The C:\Users\yourusername\AppData\Local\Temp\License Manager_reg.log shows signature problems on certain dlls.

Follow the steps below to update any certificates for .dll files that are listed as a problem in the License Manager_reg.log file.

1 - Run the following command(as Admin) to download the latest certificates in an SST file(requires internet, then you can transfer the file to the offline VM):

certutil.exe -generateSSTFromWU roots.sst

2- Open Powershell as admin and run the following commands: (You can open the roots.sst and install one by one the certificates that you require)

$sstStore = ( Get-ChildItem -Path <em>CertPath</em>\roots.sst)

$sstStore | Import-Certificate -CertStoreLocation Cert:\LocalMachine\Root

Example:

257920_IMG