Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Ecostruxure Process Expert [2021]: How to Auto Refresh Alarms in Summary page of SA GPL
This knowledge base article explains user on how to configure auto refresh of summary alarms in Summary page of Situational Awareness GPL template.

By default, the Summary Alarms in Summary page of SA GPL style will not refresh automatically when page is open state. To refresh Summary page, User must navigate to other page and open Summary Alarms page again or need to manually click on Summary Alarm page navigation again.
This is designed to minimise the load on Alarm server. If User needs auto refresh mechanism for Summary Alarm page, please follow the procedure given below.

1. Create a Cicode function as shown below.

pic1

So, this Cicode function will sleep 5 seconds and then call the SOE page. This will be refresh period.

Then you should change the "events" inside the properties for the SOE page. Use the On Page Shown to execute the function while you are on this page.

pic2

There is a big disadvantage here.

If you are scrolling or filtering the historical events, it will reset the page and bring you back to the top. So, you can't scroll through it.

To avoid this you can add a button to toggle the state between the refreshing and non-refreshing. User can scroll to the Alarms after setting to Non-Refreshing state by clicking on configured button as shown below.

pic3

pic4

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre