Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I Use Regular Modbus to Collect Realflo Liquid Run Daily/Hourly History from a SCADAPack?

At the present time, gas runs have the ability to present data to a SCADA host in regular Modbus and Enron Modbus. If using liquids, ONLY Enron Modbus can be used to collect liquid run history records/alarm/event data.

The Geo SCADA Realflo driver supports all run types and all run data via the Realflo driver.

Since the release of Realflo 7, a list of all Modbus and Enron Modbus registers are available in an Excel spreadsheet. It is located in the following directory when Realflo is installed on your computer.

C:\Program Files (x86)\Schneider Electric\Realflo\Help