Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to check the GOOSE simulation mode on the BMENOP0300 ?

There is a simulation mode dedicated to GOOSE communication between the BMENOP0300 module configured as client, and IED device servers.

It is activated by defaut in the IED device servers to avoid any damages when It is in a commisionning phase. When activated, the simulation mode is detected by the NOP module which will ignore automatically all GOOSE messages marked as "simulation".

We can check the GOOSE simulation status of the IED device servers on the BMENOP0300 module device DDT, inside the NOP_MODULE_MOD_INFO.CLIENT_STATE related to the IED device server. Example:

SIMULATION MODE:

Simulation Mode


NORMAL MODE:

Normal Mode

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: