Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Control Expert v15.3 crash when displaying on ultra wide screen resolution 5120 * 1440
1- Issue:
Control Expert v15.3 crash when displaying on Ultra Wide screen resolution 5120 x 1440.

2- Product Line
Control Expert v15.3

3- Environment:
Windows 10

4- Resolution:
The maximum supported resolution for Control Expert v15.3 is 2560 x 1440 with Scale and Layout at 125%.
The resolution 5120 x 1440 will be supported in Control Expert v16.0

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre