Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do I need a starting capacitor when using an ATS480 Softstarter?
Issue:
Is there a need for start capacitor on the motor when starting it with ATS480?

Product Line:
ATS480, Altistart 480

Environment:
All

Cause:
NA

Resolution:
A capacitor is not needed when running the motor with an ATS480 Softstarter. The Altistart ATS480 does the soft starting itself.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre