Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Replacement Battery Cartridge Locking Tabs for Single Phase Smart-UPS

Issue:
Customers are having issues removing an RBC (Replacement Battery Cartridge) from the UPS or Extended Battery Pack.

Product Line:
Single Phase Smart-UPS

Environment:
All Serial Numbers

Solution:
Certain RBCs for Smart-UPS have locking tabs that prevents the RBCs to be fully pulled out as a safety feature. The user needs to press down on the tab groves first before pulling out the RBC. See sample below for an APCRBC115.
APCRBC115 Locking Tabs

NOTE: You may encounter issues that the locking tabs will not push down. This can happen when the batteries inside the cartridge are swollen. In cases like this, a UPS replacement may be applicable. Always check your battery life span and do not exceed the recommended life span to avoid this from happening. Refer to the FAQs below for more info.

What is the expected life of my APC UPS VRLA battery?
https://www.apc.com/us/en/faqs/FA158934/

Single Phase UPS Basic Life Expectancy - When to consider a new unit over a battery.
https://www.apc.com/us/en/faqs/FAQ000265093/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre