Issue:
Customers asking why there is no Input Power Cord or it is missing
Product Line:
Easy UPS SRV 3000 VA
Environment:
All Serial Numbers
Cause:
There is no information in the User Manual about the wiring specifications.
Resolution:
The SRV3KA does not come with an Input Power Cord out of the box. Rather, it has an Input Wiring Block located at the back.
For proper installation and operation of the UPS, it is recommended to hardwire the UPS to a 30A breaker using a 10 AWG wire.
Alternatively, an open ended input power cord with a NEMA L5-30P (3 x 10 AWG) can also be used.
For further assistance, please contact the Customer Care Center at https://www.apc.com/us/en/support/
Released for: Schneider Electric Saudi Arabia