Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Hyperlink Navigation Issue in Power Advisor PDF Reports on Chrome Versions 126
Issue

When clicking hyperlinks in the Table of Contents of Power Advisor PDF reports, generated Chrome version126 and 127, the hyperlink does not navigate to the corresponding section of the report. In some cases, it navigates directly to the end of the report.

Product Line

Power Advisor

Environment
This issue has been observed when using Chrome version 126 and Chrome Beta Version 127.

Cause
The issue is due to the PDF not being rendered correctly in Chrome versions after 125. More details can be found at: https://issues.chromium.org/issues/341973428

Resolution/Workaround
Users can continue using the older Chrome version 124. Alternatively, they can use Chrome Dev version 128 to generate Power Advisor PDF reports for now, until Chrome releases a fix for its PDF rendering issue.

Note
For information on the Chrome release schedule, please refer to Chromium Dash

To download Chrome Dev version, please go to https://www.google.com/intl/en_ca/chrome/dev/