Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I downgrade the firmware of M241 to v4.0.6.26?
Issue:
Why I cannot downgrade firmware to V4.0.6.26 on M241?

Product Line:
Modicon M241

Environment:
Controller Assistant

Cause:
The firmware V4.0.6.26 cannot be loading to the M241

Resolution:
The new M241 comes with new hardware version and is not compatible with v4.0.6.26. Customer will need to update firmware to v4.0.6.41 or greater.

M241