Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Ways to format an APC by Schneider Electric Network Management Card (NMC 2 and 3 only)

Issue:
What are the ways to format or reset an APC by Schneider Electric Network Management Card (NMC) back to defaults or factory settings?

Product Line:
NMC2 and NMC3 (AP9630, 31, 35 - AP9640, 41, 43)

Answer:

Sometimes issues may render a network management card unusable and/or inaccessible. APC by Schneider Electric provides ways to resolve such issues. A format on an APC by Schneider Electric NMC is a useful procedure in case of the following  :

  1. A card becomes unresponsive and/or is with a possible corrupted firmware.
  2. The password for an APC by Schneider Electric NMC has been lost and/or forgotten.
  3. If an end user wants to reset the card and ALL of its settings permanently to defaults.


A format does not only reset the card but, also attempts to recover from a firmware issue. This procedure is not available on an APC by Schneider Electric NMC 1 (ap9617, ap9618, ap9619) or the legacy ap9606.

Section 1 Manual :

NMC2 (All firmware)

Press and hold the NMC reset button. The LEDs will quickly flash alternating until they turn off completely. This will take approximately 25 to 30 seconds.
An image showing where the reset button is on an APC by Schneider Electric NMC2 AP9630 and AP9631
NMC3 (All firmware)

Press and hold the NMC reset button. The LEDs will quickly flash alternating until you see a solid amber light on the status LED  This will take approximately 25 to 30 seconds.
A sample image showing the location of the reset button on an AP9641 NMC3

Section 2 Through standard command line (SSH / Telnet / Direct Connection ):
NMC2 or NMC3 (All firmware)
  1. Enter the command line either by Telnet / SSH or Direct Connection (This is also outlined as a part of FAQ FA156064 )
  2. Once on the APC prompt, issue the "format" command
  3. The system is going to ask a confirmation. Respond with "YES" to continue or just press ENTER to cancel
  4. You may issue a "REBOOT" command
  5. The NMC will take a couple of minutes to complete the reboot and format process
An image showing the command line format method

Section 3 Through BOOT MONITOR command line ( Direct Connection ):
NMC2 (6.X Firmware and above)
  1. Enter the command line via Direct Connection using Teraterm (This is also outlined as a part of FAQ FA293874 )
  2. Once on the BM Prompt, issue the command "factory_reset"
  3. The system is going to ask a confirmation. Respond with "factory_reset_confirm" to continue
  4. The NMC will take a couple of minutes to complete the reboot and format process
  5. Issue a "boot" command to return to the normal APC command console
An image showing how to do a format / factory reset on an NMC in Boot Monitor

NMC3 (all firmware)
  1. Enter the command line via Direct Connection using Teraterm (This is also outlined as a part of FAQ FA293874 )
  2. Once on the BM Prompt, issue the command "format"
  3. The system is going to ask a confirmation. Respond with "yes" to continue
  4. The NMC will take a couple of minutes to complete the reboot and format process
  5. Issue a "boot" command to return to the normal APC command console
Image showing how to format an NMC3 using Boot Monitor


If you have any clarifications and/or requests for the above mentioned available information, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre