Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Smart-UPS Ultra 5kW Output Turns Off When Transferring to Battery Operation

Issue: The output of Smart-UPS Ultra 5kW UPS models may turn off during low or high input voltage conditions when the UPS is transferring to battery operation.

Product Line: SRTL5KRM2UI, SRTL5KRM2UT

Cause: If an input over- or under-voltage occurs while the UPS is transferring to battery operation mode, the UPS output may turn off in certain conditions.

Resolution: The latest firmware version improves the ability of the UPS to handle input events while the UPS is transferring to battery operation. Refer to FA170679 or FAQ000242942 to update the UPS firmware.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre