Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I clean up in an EcoStruxure Energy Hub organization, a panel server topology published in the Cloud by EcoStruxure Power Commission ?
Issue:
Panel Server Topology published to SE cloud since Ecostruxure Power commission is not supported in EcoStruxure Energy Hub (EEH) and lead to the non-logging of measurement in the cloud database.

When the issue occurs:
Panel Server Topology published to SE cloud by Ecostruxure Power commission (button "complete manufacturing" )is not supported in EcoStruxure Energy Hub (EEH) and lead to the non-logging of measurement in the cloud database

Solution:
The procedure below explains how to completely clear the Panel Server topology in EEH before republishing the topology from the Panel Server web page and reassociating it in EEH.
The original EcoStruxure Power commissioning project is not required to perform the procedure.
The engineer must: have an EEH administrator profile to be able:
-  to edit the configuration in the EEH>configuration view
-  to log in to the Panel Server web page for topology publishing.

Step 1: Go to EEH> Setup>Communication View then click on Delete Gateway
image step1

Step 2: Go to EEH>Setup>Asset View then delete the Panel board named “Switchboard”
image step2

Step 3: In the same view ( EEH>Setup>Asset), delete all the Energy meters previously attached in Switchboard.
image step3

After completely removing all the entries which are previously created from topology, Engineer can claim again the PAS without any issue.

Step 4: Re-publish the topology since Panel Server web pages
image step4

Step 5: Now claim again the Panel Server in EEH
image step5

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre