Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you share existing metering CT's with an AccuSine PCS+?
Issue
There may not be room in the switchgear for another set of CT's so it is possible to use an existing set CT's.  An example would be if there is a set of CT's for a power meter already installed in the gear.

Product Line
AccuSine PCS+

Resolution
Attached is an example wiring diagram showing how the existing metering CT's can be wired to the AccuSine from the power meter.  These CT's need to be wired in series to the AccuSine from the power meter.  It will not work correctly if wired in parallel.

Schneider Electric Saudi Arabia

Attachment(s)
PCS+ Share CT's with meter.pdf [335.61 KB]