Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
VMware host fail to enter maintenance mode due to powered on VM/s.

Issue:
If there are duplicate VMs with the same hostname, such as "localhost," this can sometimes result in VMs being incorrectly identified as system VMs and skipped for shutdown, which prevents hosts from entering maintenance mode.

Product:
PowerChute Network Shutdown

Environment:
VMware vCenter Server and ESXi hosts

Cause:
Duplicate VMs with the same hostname assigned.

Solution:
Ensure that all VMs are correctly configured with a unique hostname.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre